STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! hard fault during flash programing

hi. i am trying to save a data into stm32h7b0vbt6 flash memory. so i have used HAL_FLASHEx_Erase to erase one of the sectors and HAL_FLASH_Program to program it. it works and flash will be programed.but when debuging, code gets stuck to while of the ...

Screenshot 2025-04-27 221957.png Screenshot 2025-04-27 222042.png Screenshot 2025-04-27 222127.png Screenshot 2025-04-27 222210.png

STM32F103 BLUEPILL IS NOT DETECTING

Dear STM32 Bluepill Community,I recently acquired an STM32 Bluepill development board and have been attempting to establish a communication link with my computer via the USB interface. Unfortunately, my computer is not recognizing the COM port associ...

Resolved! Error in initializing ST-LINK device in all boards

i have been using stlink v2 for a while now, but today it wouldn't connect with any of my stm32 boards the error mesage that apears is STMicroelectronics ST-LINK GDB server. Version 7.9.0Copyright (c) 2024, STMicroelectronics. All rights reserved. St...

Resolved! UNIQUE ID

HiIs the UNIQUE ID of the STM32H562RIT6 microcontroller, which consists of 96 bits, entirely variable, or does it include fixed bits as well? Which bits are fixed?

Resolved! SPI transmit question/issue

Hi,I have a custom board which has an STM32F446RE with implemented SPI peripheral that should communicate with MAX22530 chip. Currently, I am trying to test the SPI interface but am running into something that looks strange.The SPI ioc configuration ...

70nKA_0-1745606966822.png 70nKA_1-1745607051310.png byte.jpg
70nKA by Associate II
  • 1204 Views
  • 2 replies
  • 1 kudos

STM32H743 BLDC use Hallsensor get speed(HAL)

LED1_TOGGLE();cant run when i start BLDC. can someone solve it? status of HAL_TIMEx_HallSensor_Start_DMA is OK and Mspinit is OK.void hall_init(void) { __HAL_RCC_DMA1_CLK_ENABLE(); __HAL_LINKDMA(&g_htimx_handle, hdma[TIM_DMA_ID_CC1], g_hall_d...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.