STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 with 32bit bus SDRAM GPIO assignment

Hi,Can I connect a 32bit bus SDRAM to STM32H7 and assign the FMC IOs as I wish or should I stick with the Alternate functions of the GPIOs?Specifically:  can I map 32 GPIOs to STM32H7 models with 144 LQFP package where the GPIO for D31, D30 etc.... (...

nadavb_1-1746460942702.png
nadavb by Associate
  • 1017 Views
  • 1 replies
  • 1 kudos

SD Card over SPI

Hi I have an SD card working on a Nucleo-F439 board, but I can’t get it to work on the Nucleo-H729. I'm using the code from https://deepbluembedded.com/stm32-sd-card-spi-fatfs-tutorial-examples/, but I receive no response on the SPI interface during ...

MFäh.1 by Associate II
  • 1346 Views
  • 2 replies
  • 0 kudos

SPI+GPDMA Configuration

 Besides, I don't know whether this configuration of MX is correct. /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_GPDMA1_Init(); MX_SPI2_Init(); MX_ICACHE_Init(); MX_I2C1_Init(); MX_RTC_Init(); /* USER CODE BEGIN 2 */ ...

OrionJ_0-1746351004149.png OrionJ_1-1746351030780.png
OrionJ by Associate II
  • 859 Views
  • 1 replies
  • 0 kudos

What is the speed of SRAM in STM32H7?

The STM32H743 datasheet section 3.3.2 states that the TCM memories are zero wait state, implying that they run at the core speed of up to 480MHz.  It does not make any claim about the rest of the SRAM.  Figure 2 in the datasheet shows all the AXI and...

TomCV by Associate
  • 1509 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H7B0 has a lot of spikes on the ADC signals

Dear,Setup:We using a STM32H7B0 100pins.We use 1 ADC input at 1M samplesConfigured as 16bit, differential input, with an offset of 32768.We use a Vref of 2.5V.The other side of the differential input is 1/2 of Vref (buffered with a opamp)To sample th...

OGhis_0-1734355809049.png
OGhis by Senior
  • 6645 Views
  • 12 replies
  • 3 kudos

How to connect led?

I just bought stm32 and i cant find any guides how can i enable led. I flashed pin PB7 so that it would output current

1000008815.jpg
Krafti by Associate
  • 988 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.