STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H503 OTP BUG

Hello everyone, I encountered a problem with overwriting OTP memory both from a user application and from the stm32 programmer.I write data to the OTP cell, close the memory using standard hal functions, turn off the power of the debug board, turn on...

OTP_BUG.jpg
Mike1992 by Associate III
  • 2126 Views
  • 4 replies
  • 1 kudos

Resolved! STM32L412KBU3 DFU

Need some clarification on implementing the DFU functionality on STM32L412KBU3.According to the note in AN2606 (page 350), it states: "VDDUSB IO must be connected to 3.3 V" however, on the STM32L412KBU3 (UFQFPN32) the VDDUSB pin does not exist.Curren...

question about STM32G474 dual banks

I have a test question about STM32G474 dual banks to ask :A test program for LED flashing has been successfully constructed in the IAR environment.Use STM32CubeProgrammer to load BANK1 starting from 0X8000000, DBANK=1,BFB2=0, and the program runs OKW...

STM32H503 UART bootloader read protection

Hello everyone, please advise, I encountered difficulties when removing and installing memory read protection when programming h503 via the built-in UART bootloader.I use commands {0x92, 0x6D} to remove read protection and {0x82, 0x7D} to install rea...

Mike1992 by Associate III
  • 3060 Views
  • 5 replies
  • 2 kudos

STM32H7B0 has incorrect ADC scale

Dear,We are using the ADC2 in 16-bit resolution at 100 kHz, operating in differential mode.The internal voltage reference (Vref) is set to 2.5 V.A 1 kHz sine wave with a peak-to-peak voltage of 2.5 V (ranging from 0 V to 2.5 V) is applied to the ADC ...

OGhis_1-1746199734945.png OGhis_0-1746199662145.png OGhis_2-1746199793804.png
OGhis by Senior
  • 4502 Views
  • 12 replies
  • 0 kudos

Resolved! First ISR of the timer is exected even after it is reset

Hello,I am trying to implment MODBUS Slave RTU with STM32F030C8T6. I havce used RS485 for physical layer for communication.As per MODBUS protocol, a stream of 8 bit data will be sent from Master.  As a first step slave must capture all the data in an...

Anesh by Associate III
  • 3784 Views
  • 4 replies
  • 3 kudos

Please make infographics usable again

In order to make informed decisions on chosing a mcu model, we need... well... information.The older STM32-family infographics contained a fair amount of information about what to expect in terms of available peripheral mix from a given family and it...

waclawekjan_1-1746089053595.png waclawekjan_2-1746089255739.png

Resolved! stm32H753 vs stm32H733

Hi I just wanted to ask which of the two processors is actually more powerful. The H733 seems faster, but according to Google AI, the H753 offers better performance :). What’s your take on it? Thank youBR 

MFäh.1 by Associate II
  • 1309 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.