STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Watchdog over ~22 seconds on STM303RE

Hi,Looks like I cannot get the wd over a ~22 seconds watch time .I would like the watchdog to bark every 60 seconds or more.The 303 header file specify the reload max 0xFFF and as well the window, though they are 32bit values .Also the max prescaler ...

Marius CO by Associate III
  • 873 Views
  • 1 replies
  • 0 kudos

Resolved! How to trigger a timer to start from an external rising edge?

Hello,for a measurement task, I have to perform an ADC readout a certain time after a rising edge occurs from an external device.My idea was to use the HRTIM with an external event but I am unsure if it is possible to trigger a timer start with an EE...

AndiAndi by Associate II
  • 4820 Views
  • 3 replies
  • 0 kudos

USB HOST MSC + CMSIS V1

Hi all,i succesfully tested USB HOST drivers in standalone mode on a Nucleo-F746ZG.In my application i need to use CMSIS, but i can't figure out how to make it work. I am using the same application that i use on the standalone mode but this time i pl...

AGaru by Associate III
  • 1342 Views
  • 1 replies
  • 0 kudos

STM32G0, DAC, 4095 or 4096

Using NUCLEO-G071RB board and therein DAC_OUT1, PA4, CN8.3.Use internal Vref with 2500 mV.Calculating DOR from a dst_voltage using equation in Reference Manual ​(page 360/1223)  DOR = DACoutput * 4096 / Vref gives voltages3..5 mV  too high, e.g.//  4...

JuM by Senior
  • 1156 Views
  • 1 replies
  • 0 kudos

Hi, I am trying to use STM32H745XI in my design, I have some doubts in the power supply section in the reference manual en.DM0017687!

I am trying us STM32H745XI controller in my design, I want some clarification in the power supply section. In Reference manual en.DM00176879->section 7.Power control (PWR) ->Figure22->4.External SMPS Supply, Supplies LDO. I am not understanding how t...

ARedd by Associate
  • 1237 Views
  • 0 replies
  • 0 kudos

STM32H743 Failure behavior with external core SMPS

Greetings,right know we are evaluating some strategies to reduces overall power consumption of our product, including two STM32H743 microcontrollers.Due some other design restrictions the following options are not feasible:Switch to a low power µCUse...

SCoen by Associate
  • 2060 Views
  • 2 replies
  • 0 kudos

Resolved! Getting Started Nucleo-64 STM32L412

I cannot get debugging working through the STM32CubeIDE. I can program the device using the OpenOCD debugger (but stepping through the code gives an error). However, I want to use the ST-LINK GDB server as the debugger, which does not work. I receive...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.