2019-09-06 2:24 AM
Hello,
for a measurement task, I have to perform an ADC readout a certain time after a rising edge occurs from an external device.
My idea was to use the HRTIM with an external event but I am unsure if it is possible to trigger a timer start with an EEV.
I am using a STM32H743ZI currently on a Nucleo board with CubeMX with the MCU package 1.5.0.
Solved! Go to Solution.
2019-09-09 7:28 AM
Thanks for your help. I know that the HRTIM is kind of complex for the task but I can take advantage of some of its functionality for other parts of the measurement.
I solved the problem by using the Sync functionality, connecting my signal to HRTIM_SCIN. The timers I use are configured to start on sync and it is working as expected.
2019-09-06 12:29 PM
IMO HRTIM is way too complicated for this simple task which can be accomplished by any normal timer.
See for example the [CubeH7]\Projects\STM32H743I-EVAL\Examples\TIM\TIM_OnePulse example, and there are surely more such. Combine this with ADC being triggered from timer, there are also examples for that.
I don't use Cube/CubeMX.
JW
2019-09-06 12:30 PM
Take normal timer and connect the external signal to TIMx_ETR pin.
Set timer slave mode to "trigger" or "combined reset + trigger" mode and set trigger source to ETR.
2019-09-09 7:28 AM
Thanks for your help. I know that the HRTIM is kind of complex for the task but I can take advantage of some of its functionality for other parts of the measurement.
I solved the problem by using the Sync functionality, connecting my signal to HRTIM_SCIN. The timers I use are configured to start on sync and it is working as expected.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.