2019-09-08 2:36 PM
I cannot get debugging working through the STM32CubeIDE. I can program the device using the OpenOCD debugger (but stepping through the code gives an error). However, I want to use the ST-LINK GDB server as the debugger, which does not work. I receive the following error:
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
I am incredibly frustrated with the lack of clear material for getting started. I was expecting to purchase the board, install any necessary drivers/tools, install the IDE, and start stepping through an example project. I prefer not to use the uVision IDE and was hoping that I am just not configuring the STM32CubeIDE correctly.
Solved! Go to Solution.
2019-09-08 3:58 PM
Well, nothing like figuring out your problem right after you post. For anyone else who is having the same problem, here is the solution:
I started blindly trying to program STM32Cube example projects for my board. These projects had the GPIO misconfigured and it was messing up the debug connection. After starting a new project and correctly selecting the debug pin options in STM32CubeMX and using the OpenOCD debugger to program the device, there were no more issues.
I think that it should be made more clear how to work with these example projects on the Nucleo-64 boards with clear examples on how to load and step through example code.
2019-09-08 3:58 PM
Well, nothing like figuring out your problem right after you post. For anyone else who is having the same problem, here is the solution:
I started blindly trying to program STM32Cube example projects for my board. These projects had the GPIO misconfigured and it was messing up the debug connection. After starting a new project and correctly selecting the debug pin options in STM32CubeMX and using the OpenOCD debugger to program the device, there were no more issues.
I think that it should be made more clear how to work with these example projects on the Nucleo-64 boards with clear examples on how to load and step through example code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.