STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Question about access internal flash on STM32H7

My codes are stored on bank2 and I am trying write some manufature data into BANK2 (sector 14) of internal flash.Howerver it always fail in erase stage dut to the flag of PGSERR is raised.If I change to write data to bank1 (sector7) this symptom not ...

jorgewu by Associate
  • 812 Views
  • 0 replies
  • 1 kudos

STM32f469 - ADC accuracy

Hello , We are interfacing Analog Accelerometer with STM32f469. Attached here ADC interface hardware and ADC firmware (configuration) for your reference . Problem is Accuracy with ADC values. The ADC values are varying approximately 30mV . Can anyone...

BSR by Associate II
  • 3287 Views
  • 4 replies
  • 0 kudos

STM32 internal ADC for reading temperature.

/*I want to read stm32 temperature using ADC1 with timer 2 configured. I am getting temperature reading as 60 degrees when I configured ADC1->SQR3=16; and -275 degrees when ADC1->SQR3=18; Is any thing wrong? */   #include "stm32f4xx.h" //...

0690X00000Arun6QAB.png 0690X00000ArunFQAR.png
Kumar B by Associate II
  • 6351 Views
  • 10 replies
  • 0 kudos

UART Emulation on stm32f0 series?

Hello. I know that UART emulation is possible for stm32f4 series but is there any implementation for the same using stm32f0 ?Copying the same h and c source files into the project does not work as it has too many DMA dependencies and I observe the HA...

How to calibrate ADC on STM32F767NGH

Helloi'm looking for a way to use self-calibration on STM32F767 ?i find in documentation HAL_ADCEx_Calibration_Start function, but i don't have it in HAL driver...thanks for any supportBest regards

stm32 can Acknowledgment Error

I am working with stm32f04c6 microprocessor.I've already sent data with canbus. now it does not work. status (tsr) code terro bit 1 is.there is no ackCAN error status register (CAN_ESR)LEC[2:0]=011; 011: Acknowledgment Error what should i do?////can ...

Communication between two FDCAN members and a third member transmit a CAN-FRAME which the two others should ignore. The thrid member ignores FDCAN-Messages

Hello everyone,I am using the NUCLEO-144 Board with STM32H743ZI.I would like to test the FDCAN with three members. Two of them use the FDCAN. The third one is an uC which accept FDCAN but cannot do anything the message of the two others. If I send me...

MSchn.14 by Associate
  • 906 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.