STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

iolink support for STM32L452

Dear All,We have our custom board in which we used STM32L452 chip. Now we want to access this board as iolink device.we have one reference code of "STM32L073RZ-Nucleo", so can anyone help us to port example code for our board means STM32L452 chip?Tha...

How much of a frequency drift of the driving clock from the grandmaster source clock will cause the "Incorrect flexible PPS output interval under specific conditions " errata to occur?

Our desire is to use the flexible PPS with fine correction for synchronization purposes. We are wondering if it might be possible to avoid the incorrect flexible PPS output interval with a quality grandmaster. Is it possible to get a clarification of...

DFSDM latency

We are using the STM32f413 with the DFSDM unit for converting the PDM stream generated from the external ADC. The clock is generated externally. We are using the OSR of 512 and sinc3 filter with an integration time of 8, a regular channel with contin...

AndrejC by Associate
  • 1284 Views
  • 1 replies
  • 0 kudos

Resolved! How to change the linker file for STM32H743 to support using the whole 1 MB of RAM for the code execution?

Here is the content of stm32h743xx_flash.icf:define symbol __ICFEDIT_region_ROM_start__   = 0x08000000;define symbol __ICFEDIT_region_ROM_end__    = 0x081FFFFF;define symbol __ICFEDIT_region_RAM_start__   = 0x20000000;define symbol __ICFEDIT_region_R...

EAbu by Associate
  • 2453 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.