STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Howto: Firmware Version Handling?

I'm new at stm32 processors and have a question about firmware handling. At the moment I'm using an uint value for the firmware version and it seems not to be the correct way. So what's the right way for doing this? Is there a register where I can sa...

STM32H743 UART read/write to/from PC and MCU

Hey there,I was wondering where I could find some resource materials for configuring UART to read and write to serial or if I could get a hand with it. Using CubeMX, I've enabled USART3, USB_OTG_FS, and and the USB CDC middleware, but still can't see...

Resolved! [STM32L431] Cannot monitor VBAT using ADC

I am trying to read VBAT value through channel ADC1_IN18.VBAT should be between 2.3 and 3.3V.VREF+ pin is connected to VDDA=1.8V.Values measured using ADC are linearly related to the real VBAT value, but I have not been able to get the exact value.Fo...

TClar.18 by Associate II
  • 4658 Views
  • 9 replies
  • 0 kudos

SDIO (with DMA) does not respond after inactivity

Hello to the community!I've run into a strange problem on my STM32F7:I init, mount and open a file directly after the uC initif I read this file often (from my main() while(1)), I never have read problems (it can works for hours)if I don't read the f...

jean by Senior
  • 827 Views
  • 0 replies
  • 0 kudos

Can Bus store message

Hi all, I’m trying to test the can bus function with the STM32F042, I’ve studied all the Datasheet but I’m trying to find the best solution for an efficient store for incoming messages..My question is if I don’t know the right amount of incoming ID ...

STM32L452xx: Memory mapping calculation

Looking at the datasheet of the STM32L452xx family, it's noted that SRAM size is 160K.The memory mapping on page 86 notes the address range from 0x2000'0000-0x2028'0000.But 160K is 0x2'8000 and not 0x28'0000, which would make the range from 0x2000'00...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.