STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

unknown memory region

I used mac and st-flash v1.5.1 to download .bin file to B-L475E-IOT01A1, but I got "unknown memory region", could anyone help me to solve this? Thanks

wxie by Associate II
  • 3145 Views
  • 4 replies
  • 0 kudos

Which MCUs support 32.768MHz in SAI slave mode?

I have been trying to get the AD7768-4 to work with an L431.I (belately) realized that the maximum SAI slave clock speed in the L4 is 25MHz. It appears that the APB1 clock speed is the limiting factor. I could potentially achieve 192ksps by replacing...

0690X00000BuyMNQAZ.png

How to disable UART temporarily?

Hi,i send data to STM32F4 from STM32F0. then i send these values to thingspeak using ESP8266. but it works onle once. after i send values to thingspeak using ESP8266 it returns endless trash values via UART2. and i can send data from F0 to F4. so i h...

STM32 ADC problem

I am using STM32F030F4P6 when I call this Function my ADC starts successfully and I can read ADC value in ADC callback but my MCU hangs at this function line what is the problem? My code is generated by st32mcubemx and my IDE is IAR. I have a problem...

AAg.14 by Associate
  • 2432 Views
  • 2 replies
  • 0 kudos

Resolved! RN4020 Uart Communication with Stm32L100 Discovery Board

Hi,I am trying to communicate RN4020 with my STM32L100 disco board however I could not manage to do it. I can send commands and get AOK and Reboot responses when I try it with an Arduino. I did monitor that Disco can communicate correctly with Arduin...

herca.1 by Associate II
  • 1753 Views
  • 2 replies
  • 0 kudos

Oryginal H750

Hi! I want to buy ~cheap​ but oryginal STM32H750.Are there fakes and how to spot them? What is target ID of *vbt6 chip?​On china market this chips costs 1/2-1/3 the price than in quite reliable seller in my country.​Im hobbyst so I first consider rel...

oeliks by Senior
  • 938 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.