STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is it possible to obtain 32 channels (single ended) of 16 bit AtoD conversion (15KSmps per channel), and set individual per-channel gain with onboard OPAMP in PGA mode?

The idea is to change PGA gain before every conversion, but I can't find any info about the time that PGA needs to change the gain.Manual states that it is possible to have up to 36 16bit channels of ADC. Manual states that PGA could be attached to A...

SD.11 by Associate
  • 686 Views
  • 0 replies
  • 0 kudos

We can add DMA interrupt for the stm32f042x6 ?

We have 3 DMA interrupts  DMA1_Channel1_IRQHandler, DMA1_Channel2_3_IRQHandler, DMA1_Channel4_5_6_7_IRQHandler, i need use 3 interrupts beer 2 channels because i use 3 usart with DMA (3 x channels for TX and channels for RX). 1- i can split the chan...

Configuring ADC and DFSDM on Nucleo-H745

Hello!The what I want is to configure the ADC 16-bit synchronous sampling from 2 ADCs and 6 Sigma-Delta using DFSDM at 1kHz period on M4 core to circular buffer. I'm not sure how to do it right, but I'm suppose that I need to enable say TIM1 at 1kHz ...

Alex.Ag. by Associate II
  • 972 Views
  • 0 replies
  • 0 kudos

Resolved! Pwm vs timer irq - slow 100khz max

Hi ! Im generating pwm at 200khz with no problems. But when I use ​timer to generate interrupt I get max 100khz of pulse on pin. No matter if I use HAL_GPIO_Toggle/WritePin or just GPIOx->BSRR. No matter how low value of timer prescaller I use.​Outpu...

oeliks by Senior
  • 1743 Views
  • 5 replies
  • 0 kudos

Resolved! How to configure CAN interface on STM32F042F6P6?

Hi!I am confused, i wanted to use STM32F042F6P6 MCU for can interface but, ther is no TX pin for can interface (PB9 on datasheet). So, how i can configure CAN TX?There is no CAN mode option for this MCU inside of CUBEMX because there is no TX pin for...

BMama.1 by Associate
  • 1621 Views
  • 2 replies
  • 0 kudos

STM32F103RDT6 Uart details

Hi team,I am using STM32F103RDT6 for my project. I would like to know the details of UART in the MCU. in the datasheet it shows 5 USART interface is possible. At the same time 2 UART is also mention in the datasheet.So my doubt is that can I use the ...

Mom.1 by Associate II
  • 708 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.