STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Microsecond delay using timer in stm32L0

I want to generate the microsecond delay for stm32l083cz.when I using the configuration PLL clock ...32Mhz freq to APB1 which is connected to timer2 PSC -- 32-1 and Period 0xffff-1 Its working perfect and i am able to generate the microsecond delay.B...

Resolved! First timer delay missing -- AN4776 wrong?

I'm new here but have already gotten lots of good advice, so I'll press my luck and ask another question. Can't believe it hasn't come up before, but search doesn't find anything.Simplest possible timer example. Start counting down from ARR value, bu...

Resolved! Timer Configuration

Hi, I am using STM32F779NI for development. My requirements are:On PD15, i.e Timer 4 channel 4, I want to generate a PWM output.On PB7, i.e Timer 4 channel 2, I want to use it as an Input capture functionality.Is it possible to configure the Timer fo...

A3 by Associate III
  • 4217 Views
  • 10 replies
  • 1 kudos

PWM -> ADC & DMA

Hi, I want to​ trigger ADC with PWM, transfer it to array by DMA.​But first I have problem with setting dma.​......​Question 1.​Do I have to start HAL_ADC_Start before I use HAL_ADC​_Start_DMA​Or will this second function start adc & dma?

oeliks by Senior
  • 887 Views
  • 1 replies
  • 0 kudos

f103 LL spi DMA not interrupted

hii use f103 to read ad7606 with spi i see cube example for LL( hal spi has delay)i want read two out of a2d so i config spi1 master receiver and spi2 slave receiver clk of spi1 and spi2 and a2d connect together out A connect to spi 1 and out 2 conn...

MacLaren by Associate III
  • 883 Views
  • 0 replies
  • 0 kudos

STM32F030F4P6 EMI problems?

Hi,I designed a board with a STM32F030F4P6 on it. The board is about 68x48 mm and contains the microcotroller a AC/DC supply and a nRF24L01 RF-Module. supplied directly with about 5V from an external supply the circuit works as it should. But when I ...

Mister232 by Associate II
  • 8925 Views
  • 9 replies
  • 0 kudos

Entering the Stop modes

Hello,I am using STM32L476 and I was just wondering how do I enter in various stop mode (modes 0, 1 and 2) please?Thanks,ALi.

mmsya by Associate II
  • 1299 Views
  • 1 replies
  • 0 kudos

STM32H753

Can anyone share project stm32h753vi with ethernet RMII ? Thanks so much

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.