STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CANFD frame format !!!!!

hello ST Community ,the frame format settings of the CANFD are missing FDCAN_FRAME_CLASSIC !!!!I can set this format only with hand in the software but as soon as i try to generate a new code this setup would be overwritten with the available setting...

Moha-Affa by Associate II
  • 1138 Views
  • 0 replies
  • 0 kudos

STM32L151C8T6 USART1 works from time to time

Hello.I'm using STM32L151C8T6 for some simple task. In the beginning I used MSI clock and everything was fine. But I decided to switch to HSI and now I got problems using USART1, namely I think that the USART1 periphery isn't properly initialized due...

kaloyan by Associate III
  • 2342 Views
  • 5 replies
  • 0 kudos

Timer Configuration for specific duration

Hello ,I want to configure a timer which start and runs for specific duration and stops automaticallyand when again i want to start that timer i could be able to start timer and agian stops automaticallyduration is fixed all timeDipak Garasiya

Timer configuration

i want to implement a timer which make a perticular pin to toggle at perticular time duration the duration could I set manaully.

FDCAN Bittiming Problem __ STM32H750 __

Hi,my question is simple , i have these parameter :Can_Clock = 48 MHz Prescaler = 1;NominalTimeSeg1 = 18NominalTimeSeg2 = 4and this is the MX_FDCAN1_Init() :static void MX_FDCAN1_Init(void) {   /* USER CODE BEGIN FDCAN1_Init 0 */   /* USER CODE E...

DAC/ADC conversion + timer triggering

Posted on January 16, 2018 at 10:34Hello,I need to control the acquisition and generation of a signal using the STM32F746ZG and its internal DAC and ADC. The idea is to trigger the DAC using one timer and the ADC using another timer (without the use...

Openocd

I ported openocd to the stm32l522. ​​https://github.com/morbos/openocd-0.10.1​openocd -f board/st_nucleo_l522.cfg​​From there you can remote connect from gdb, flash, and see the s/ns processor regs. Watchpoints work also.​Hedley​​

Hedley by Associate III
  • 1973 Views
  • 3 replies
  • 4 kudos

Not Correctly Read ADC Conversion Through SPI Interface

Hello,On my custom designed PCB, there is a STM32F7 processor. With SPI DMA interface, I try to get the converting values of the external ADC. But everytime I get 3.1V in debug session. So how can I read the correct values based on the input signal?w...

0690X00000BuqL2QAJ.png 0690X00000BuqKxQAJ.png
AE104 by Senior
  • 1565 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.