STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H745-DISCO odd SDRAM problem

Hi all,my SDRAM setup seems to work EXCEPT that I have a strange behavior:When I write any value (8, 16, 32 bit) to an address (example 0xd000004),it in fact gets written to the address - 2, in this example 0xd0000002.All written bytes are readably @...

LHohl.1 by Associate II
  • 2134 Views
  • 3 replies
  • 0 kudos

ADC multichannel question

Hi, I want to set 3 channels of adc and transfer data via dma to buffer.​But I want to read rando​mly, sometimes only ch1, sometimes only ch3 etc. One channel at time. And fill buffer with data from one channel.​​Do I have to set:-adc continous - dis...

oeliks by Senior
  • 1079 Views
  • 2 replies
  • 0 kudos

Resolved! using LFN feature in sd card with stm32f4

Hi,I want to use lfn feature in sd card and i use stm32f4 for this purpose i set _USE_LFN to 1 and _MAX_LFN to 255 . when i create the file , file is created but when i want to return file name , returns wrong.please guide me, how to return file name...

alianvari by Associate III
  • 2969 Views
  • 5 replies
  • 1 kudos

STM32F103RDT6 Pin details

Hi,I am using STM32F103RDT6 for my project. I need only two seperate uart lines and 2 Gpios for to connect 2 RS485 transceivers.I need TX ,RX pin only. So what about the CTS & RTS pin. can I make that as float?There is 2 boot pins in the IC. how I co...

Mom.1 by Associate II
  • 2353 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.