2019-12-27 1:51 AM
Hello ,
I want to configure a timer which start and runs for specific duration and stops automatically
and when again i want to start that timer i could be able to start timer and agian stops automatically
duration is fixed all time
Dipak Garasiya
2019-12-27 2:39 AM
Enable the timer in RCC. This is dependent on the MCU series, check the reference manual to see which register in RCC has the APB enable bit for the timer.
Set the prescaler (if needed) in PSC, and set the UG bit in EGR.
TIMx->PSC = prescaler - 1; TIMx->EGR = TIM_EGR_UG;Set the auto reload register (ARR) to the required timer period - 1
TIMx->ARR = period - 1;Start the timer by setting the counter enable (CEN) and one pulse mode (OPM) bits in CR1.
TIMx->CR1 = TIM_CR1_CEN|TIM_CR1_OPM;If the timer period is elapsed, (TIMx->CR1 & TIM_CR1_CEN) will be automatically cleared, the timer stops, and you can repeat the line above to start it again.
2019-12-28 3:35 AM
If I want to set timer of 5 sec , how to calculate prescaler and period
my system clock is 16MHZ
2019-12-31 12:07 AM
You need the peripheral clock frequency of the timer, not the system clock. You have already found out in the previous step which APB bus the timer is connected to, so note the frequency of that APB bus.
The frequency is the number of cycles in one second. For a timeout of 5 seconds, the required number of cycles is five times the frequency.
Most timers have 16 bit counters (check the timer main features in the reference manual), and the required number of cycles is likely greater than 2^16, so you have to factorize it into a product of two numbers, both less than 2^16. Then use one of them as the prescaler, the other one as the period.
2019-12-31 3:42 AM
Thanks @berendi
I have tried your code but i am not getting clearing register. like i am posting my code with this post
i have test to set pin high for some time to test using timer
RCC->APB1ENR |= (1<<1); // Enable clock for TIM3
TIM3->PSC = 999; // Int clk divided by 1000(999+1)
TIM3->EGR = TIM_EGR_UG; // Forcing to generate a update
TIM3->ARR = 7999; // Counts from 0 to 7999
TIM3->CR1 = TIM_CR1_CEN|TIM_CR1_OPM;
while ( (TIM3->CR1 & TIM_CR1_CEN) != 0)
{
HAL_GPIO_WritePin(GPIOH, GPIO_PIN_6,GPIO_PIN_SET);
}
Best Regards
Dipak Garasiya
2019-12-31 4:31 AM
How do you know that CEN does not get cleared? What do TIM3 registers contain when you let it run for a while and stop it? Does it exit the loop?
2019-12-31 8:00 PM
I have checked by debugging code , while loop never exits. and stops code there
i have attached my debugging sceenshot where you will get TIM3 register value at timer of entering while loop
Best Regards
Dipak Garasiya
2020-01-02 1:46 AM
I can't see the screenshot.
Check the timer registers. Do PSC, ARR and CR1 contain the values you've set? Is the counter changing?
2020-01-02 5:08 AM
What's *after* the while loop?
Put some code there, e.g. another write to a GPIO pin.
JW
2020-01-02 8:27 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.