2019-12-08 6:45 PM
I ported openocd to the stm32l522.
https://github.com/morbos/openocd-0.10.1
openocd -f board/st_nucleo_l522.cfg
From there you can remote connect from gdb, flash, and see the s/ns processor regs. Watchpoints work also.
Hedley
2019-12-20 9:23 AM
Nice!
I suggest to post your change into the official OpenOCD repository.
There a whole gerrit to review changes at: http://openocd.zylin.com
By the way, for STM32L5 there is already an existing change at : http://openocd.zylin.com/#/c/5344
You can try to find a consensus with the owner of the change, if you judge that your change is more appropriate.
Happy New Year !
Tarek
2019-12-20 10:26 AM
Hi Tarek,
Appreciate the code ptr. That version supports L5 as a new flash target. I do also. The missing piece is ARMv8m support. I handle the secure and non secure contexts. That also involved a change to the STlink hla code to make it ARMv8m aware.
Enjoy the Festive Season!
Hedley
2020-01-02 2:26 PM
I updated the openocd me. It's st_nucleo_l552.cfg dunno why I have been typoing that as 522...
The new version also supports correct flash size reading and flashing when the watermarks are used. before, if you watermark the S/NS split, the erase fails at the watermark address. The soln I found was to temporarily unlock the option bytes and default the watermarks, I dont permanently write them, it's just for the curr reset. Next time you reset, the old values take over.
I have 2 Ada programs running on the stm32l552. The first part of the flash at 0C000000 is S, then at the watermark, the NS program begins at 0802xxxx.
There is no ST sample code so I had to do this blind with just the RM and SVD file + prior L4 ports.
github.com/morbos/STM32/tree/master/L/L552/sx1276_rom_l552
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.