STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to divide word variable into 2x halfword?

Hi? I set my ADC1&2 in simultanous mode. I write these 2 data halfword to 1 - 32 bit variable word.​How can I divi​de this 32 bit variable into 2 separate variables? To get values of ADC1 and ADC2 separate?​ADC is 12 bit.​Thank You :)

oeliks by Senior
  • 5228 Views
  • 13 replies
  • 0 kudos

TouchGFX Designer, only Simulator as Application Template.

Hi,I was following the tutorial below:https://touchgfx.zendesk.com/hc/en-us/articles/205443722-Step-1-Setting-a-background-ImageAccording to the tutorial there should be the application template for the STM32F746G Discovery Kit. But the TouchGFX Des...

Asantos by Senior
  • 825 Views
  • 1 replies
  • 0 kudos

Why stm32 usb msc not work with freertos?

I use STM32746G-Discovery to learn usb msc.I copied STM32Cube_FW_F7_V1.15.0\Projects\STM32746G-Discovery\Applications\USB_Device\MSC_Standalone and it works fine.but when i use Freertos to drive msc, the PC popup a dialog that the device can't be re...

Is the STM32H743VIH6 VDDLDO pin connected internally to VDD?

The STM32H742xI/G STM32H743xI/G data sheet (DS12110 Rev 7) implies VDDLDO can be supplied separately from VDD. “When it is not available on a package, the VDDLDO pin is internally tied to VDD.�? And “VDDLDO ≤ VDD�?. However, on the STM32H743VIH6, VDD...

AMacI.1 by Associate II
  • 1216 Views
  • 0 replies
  • 1 kudos

HAL_UART_Receive_IT

Hi there!I hope someone can help me. Afther a couple of years i start again to program the STM32 microcontroller (STM32F051). I need the use a UART for trasmit and receive data. For the trasmission no problem work weel ( i use the interrup HAL functi...

SGian.1 by Senior
  • 2973 Views
  • 5 replies
  • 1 kudos

TImer triggered circular DMA SPI TX

Hi,I am trying to understand DMAMUX possibilities and usage.My target is to implement auto refresh of external muxed (scanning) SPI LED display. Just 3 shift registers in daisy chain. 1 byte selects current characters (mux) and 2 bytes are contents o...

0690X00000BvkjUQAR.png
xorly by Associate II
  • 2911 Views
  • 6 replies
  • 0 kudos

What is the Problem with my Program? (Using Mat-Target)

@The things i use:Hardware: Stm32F446RESoftware: CubeMX V.5.4 ; Matlab R2019b ; CubeIDE V.1.1 ; Mat-Target My Question is: Where is the Mistake in my Programm. I defined the PA5 as a Gpio output because that´s the Output for the LD2 LED on my board w...

Driko by Associate II
  • 2566 Views
  • 0 replies
  • 1 kudos

What does error cause 0x08 returned by ST7580 mean?

I would like to send data with modulation "B-PSK coded with Peak Noise Avoidance". Most of the time I receive instead of DL_DataConfirm a response DL_DataError with error cause 0x08. Unfortunately, that error code is not documented in user manual. Co...

MPlet.1 by Associate
  • 913 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.