2020-01-09 3:58 PM
Hi,
I was following the tutorial below:
https://touchgfx.zendesk.com/hc/en-us/articles/205443722-Step-1-Setting-a-background-Image
According to the tutorial there should be the application template for the STM32F746G Discovery Kit. But the TouchGFX Designer 4.13.0 only have the option for the Simulator.
Do templates need to be installed separately?
2020-01-09 5:39 PM
My wokstation machine only have internat in a virtual machine, using another computer with internet i was able to load new templates using the CHANGE button.
I followed the tutorial "Setting a backgroundimage", The "Run target" button loaded the code on the board and the display shows the image. But the "Generate code" button only generate code for the simulator.
How to generate the source file for the STM32F746G Discovery Kit?
Is it possible to generate code without RTOS?
How to link the GUI code from the TouchGFX Designer with the board code from the STM32cubeMX?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.