STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using STM32F413 bxCAN peripheral. Using MX HAL. From RM0430 I think I understand that the ERROR interrupts (Bus-off, Passive and warning) is generated when these flags are set. But it seems like interrupts happens more often than so.

I have enabled interrupt for BOFF, EPVF and EWGF.When e.g. sending with error the very fist time TEC becomes = 1, all flags remain 0. However I get an interrupt any way - every time I get a send error. Eventually i get flags set as REC/TEC gets large...

PÖste.1 by Associate II
  • 1461 Views
  • 2 replies
  • 0 kudos

Sampling frequency on multichannel ADC with DMA

HIi have (hopefully) set up a three channel ADC with DMA and a Timer to get a sampling frequency of 100kHz. I am wondering if somebody could t Hake a quick peek on my code to verify that it is correct. The HLCK is maxed at 216MHz, and TIM6 has a peri...

AitchJee by Associate II
  • 845 Views
  • 0 replies
  • 0 kudos

I am planning to make a custom PCB using the STM32F777NI microcontroller. I need the symbol (schematic symbol) of the microcontroller.

I am planning to make a custom PCB using the STM32F777NI micro-controller for that, I have to make the schematic for the same to make the PCB. I can't find the symbol for the micro-controller for the schematic. Where I can find the symbol of the all ...

Is it possible, after properly inizializing the FMC, write directly to an external memory without resorting to FMC functionalities?

Dear all,to explain better, what I have is an external memory connected to my stm32f4 MCU, in order to communicate with it I have to pass through the FMC. The external memory is an FPGA.What I would like to do, if it is possible, is to first iniziali...

NMaun by Associate
  • 1365 Views
  • 2 replies
  • 0 kudos

STM32F042F4P6 - Input current in trigger mode.

Help find the answer. I want to run TIM2 in trigger mode. If you connect ETR1 to Vdd, then the current at input ETR1 will be 45 mA. If you connect it to Vdd through a resistor, then the timer does not work. Where can I find a diagram of the correct c...

0690X00000BvpCQQAZ.png
MKhan.1 by Associate II
  • 3703 Views
  • 8 replies
  • 0 kudos

Resolved! Timer count of 1 ms

HelloI want to configure timer which increment count by every millisecondwhat are value of prescaller or other parameter should configure in it ?i am attaching you my clock configuration with this RCC->APB1ENR |= (1<<1); // Enable clock for TIM3 TIM3...

Resolved! STM32F103C8T6 PWM Generation

How to generate PWM so that the LED lights up for 5 seconds? Now, my LED is just blinking. I watched a lot of tutorials, but I don't know where I'm wrong. I need help...My code: #include "stm32f10x.h" #include "stm32f10x_gpio.h" #include "stm32f10x_r...

Resolved! HOW to set resolution in ADC for STM32F103VBTx

I am working on STM32F103VBTx ADC. I am using HAL drivers. I dont find the setting where I can set the resolution. In old HAL drivers we had "hadc1.Init.Resolution = ADC_RESOLUTION_12B;" this field to set resolution. But in new drivers I dont find th...

sne_123 by Associate III
  • 3324 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.