STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F469IG interfaced with 16Mb SDRAM

The STM32F469IG needs to be interfaced with the ISSI IS16100H-7TL (512K x 16 bits x 2 Banks, 16Mbit SDRAM). This SDRAM has 12 address inputs, A0 - A11.Should the SDRAM controller in the MCU being configured for 12 bit address and connect FMC_A0-A11of...

Wvan .11 by Associate
  • 761 Views
  • 0 replies
  • 0 kudos

Resolved! Reset timer prescaler counter

In my STM32H7 application I start a timer, stop it in an update interrupt handler (by setting ARR to 0), then when appropriate I set a new ARR value thus restarting the timer. This happens very frequently. During each such period I execute a number o...

manx by Associate III
  • 5804 Views
  • 5 replies
  • 3 kudos

Current consumption in VBAT mode

Hi,I am using STM32H753 controller in my design, I am measuring the current consumption in vbat mode with the battery and found it to be around 1uA. The RTC Configuration was RTC_Alarm_A enabled.But disable the Alarm_A in the RTC configuration, the c...

Vel by Associate III
  • 2934 Views
  • 3 replies
  • 0 kudos

UART2 interrupt skipping received bytes

Hi everyone, i'm using uP STM32F103C8T6 processor and GPS module NEO M6Q with standard uart configuration on 9600 baud-rate .I enable global UART2 interrupt to receive data from GPS module on every second. But for some reasons, interrupt starts skip...

0690X00000BvlPBQAZ.jpg
Indu by Associate II
  • 1316 Views
  • 1 replies
  • 0 kudos

STM32L0 can't flash with FLASHER-STM32

Hello, I am using STM32L021F4 on a custom board and I am attempting to flash firmware using the FLASHER-STM32 software via the internal bootloader and a FT232RL USB/UART serial bridge. I can connect to the MCU and the flash loader says the MCU is rea...

jefflongo by Associate III
  • 825 Views
  • 0 replies
  • 0 kudos

STPM33 reference circuit. I did not understand.

I am trying to use STPM33.I am designing a circuit with reference to the reference circuit.The circuit I'm looking at is the 'EVALSTPM33' circuit from the STPM33 kit.I have two questions.1. Many circuits are falling to ground. What is the difference ...

0690X00000BvlWqQAJ.png 0690X00000BvlWvQAJ.png
LYoun.11 by Associate
  • 880 Views
  • 0 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.