2020-01-09 5:31 AM
How to generate PWM so that the LED lights up for 5 seconds? Now, my LED is just blinking. I watched a lot of tutorials, but I don't know where I'm wrong. I need help...
My code:
#include "stm32f10x.h"
#include "stm32f10x_gpio.h"
#include "stm32f10x_rcc.h"
#include "stm32f10x_tim.h"
#define Period 0xffff
#define Pulse 0
int main()
{
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO, ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
//PB1
GPIO_InitTypeDef pwmGPIO;
pwmGPIO.GPIO_Pin = GPIO_Pin_1;
pwmGPIO.GPIO_Mode = GPIO_Mode_AF_PP;
pwmGPIO.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOB, &pwmGPIO);
// TIM3, channel 4
TIM_TimeBaseInitTypeDef pwm;
TIM_OCInitTypeDef pwmOC;
pwm.TIM_Period = Period;
pwm.TIM_Prescaler = (SystemCoreClock / 4800000) - 1;
pwm.TIM_ClockDivision = 0;
pwm.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM3, &pwm);
pwmOC.TIM_OCMode = TIM_OCMode_PWM1;
pwmOC.TIM_OutputState = TIM_OutputState_Enable;
pwmOC.TIM_Pulse = Pulse;
pwmOC.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OC4Init(TIM3, &pwmOC);
TIM_OC4PreloadConfig(TIM3, TIM_OCPreload_Enable);
TIM_ARRPreloadConfig(TIM3, ENABLE);
TIM_Cmd(TIM3, ENABLE);
while(1)
{
for(int i=0;i<5000;i++){
TIM_SetCompare4(TIM3, i);
}
}
}
Solved! Go to Solution.
2020-01-09 12:24 PM
I found out what is wrong, Unfortunately my controller not working properly :( tested on another one, working well
2020-01-09 6:09 AM
> for(int i=0;i<5000;i++){
> TIM_SetCompare4(TIM3, i);
> }
What is this supposed to do? Mind, the PWM period is something like 1/72 seconds, and this loop writes the compare register like half a million times during that time.
For starter, you want something more like:
while(1) {
TIM_SetCompare4(TIM3, 0 * Period / 4);
Delay1Second();
TIM_SetCompare4(TIM3, 1 * Period / 4);
Delay1Second();
TIM_SetCompare4(TIM3, 2 * Period / 4);
Delay1Second();
TIM_SetCompare4(TIM3, 3 * Period / 4);
Delay1Second();
TIM_SetCompare4(TIM3, 4 * Period / 4);
Delay1Second();
}
JW
2020-01-09 6:46 AM
It didn't help, the LED is still blinking :(
2020-01-09 12:24 PM
I found out what is wrong, Unfortunately my controller not working properly :( tested on another one, working well
2020-01-09 11:23 PM
Thanks for coming back with the solution.
Please select your post as Best so that the thread is marked as solved.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.