2020-01-09 7:22 PM
STM32H753VI
Our product has (1) stm32h753vi in a multiprocessor system.
Processor #2 has a GPIO pin connected to NRST on the stm32h753vi with a 10K pull up.
Processor #2 will need to reset the stm32h753vi by driving it's GPIO pin under certain conditions.
On the stm32h753vi there is a:
bootloader at 0800 0000
application at 0801 0000
The bootloader jumps to the application by performing a software reset (see code below).
This was done this way to solve the problem of relocating the interrupt vector table.
On page 312/3247 RM0433 Rev 5 (STM32H753 Reference Manual)
Table 50. Reset distribution summary (continued)
This table suggests that the NRST line is being driven as an output during the software reset operation.
What I am seeing is that after the software reset is finished (the application is running ok)
NRST seems to still be an output - causing processor #2 not able to drive the NRST line all the way to low.
Question: After performing a software reset in this manner how do you change the NRST output back to being an input?
From Table 50 it would seem this same situation will apply for a watchdog timer reset as well...
Thanks in advance for your help
__ramfunc static void Jump(unsigned int address)
{
/* set the boot address after reset */
MODIFY_REG(SYSCFG->UR2, SYSCFG_UR2_BOOT_ADD0, ((address >> 16) << POSITION_VAL(SYSCFG_UR2_BOOT_ADD0)));
/* Ensure all outstanding memory accesses including buffered write are completed before reset */
__DSB();
__ISB();
/* reset */
SCB->AIRCR = (uint32_t)((0x5FAUL << SCB_AIRCR_VECTKEY_Pos) |
(SCB->AIRCR & SCB_AIRCR_PRIGROUP_Msk) |
SCB_AIRCR_SYSRESETREQ_Msk ); /* Keep priority group unchanged */
__DSB(); /* Ensure completion of memory access */
while (1) /* wait until reset */
{
__NOP();
}
}
2020-01-09 10:46 PM
NRST in STM32 is an input with an internal pullup (cca 40kOhm) and a filter, connected with an open-drain output (i.e. a single transistor switching to ground) for the internally generated resets to be propagated outwards. I doubt this is different for the 'H7.
In some STM32 NRST can be shared with an IO, but this is not the case of 'H7 as far as I can tell.
JW
2020-01-09 11:13 PM
> Processor #2 has a GPIO pin connected to NRST on the stm32h753vi with a 10K pull up.
Was this GPIO ever an active high output? That might have damaged the NRST circuitry inside.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.