STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Any differences between these two STM32F030C8T6 chips?

We need further clarification regarding the difference between the above ICs.We recently purchased the mentioned STM32 MCU, but received two different variants. In one IC, the ST logo on the right side has the marking “e3” with “L” outside the circle...

STM32.jpeg

Resolved! STM32F407 VBUS sensing detection

I am developing a device that implements the USB device class.According to application note AN4879 "Introduction to USB Hardware and PCB Design Considerations Using STM32 Microcontrollers" it is written as follows:Based on the USB specification, a US...

Alex_777 by Associate III
  • 2391 Views
  • 5 replies
  • 1 kudos

Resolved! STM32F303K8, write to SYSCFG register has no effect

I got another strange issue with a STM32F3, as usual related to DMA.The problem relates to an "old" DAC / DMA example I tried to port to a different MCU.The original is called "DMA_RAM_DAC", and is part of the V1.1.0 firmware package for the F303 dis...

Ozone by Principal III
  • 384 Views
  • 2 replies
  • 2 kudos

Resolved! stm32u073k8 No VLCD pin

I'm using the LCD of the STM32U073K8, but the program failed to initialize the LCD. After checking, I found that the STM32U073K8 doesn't have the VLCD pin. Is the STM32U073K8 not compatible with the LCD peripheral? Or are there other settings?  

ShimiaoWang_0-1769480605102.png ShimiaoWang_1-1769480620718.png ShimiaoWang_2-1769480629049.png

Firmware update stm32u535

Hi All,I've this requirement, can someone suggest how do I proceed.I'm using stm32u535 and over usart it's connected to Silicon labs chip. Silicon labs chip has Wi-Fi and I want to update firmware of STM32U535. This silicon labs chip is connected to ...

Resolved! MX25UM51245G not being initialized by bootrom

We are currently working with a custom PCB using an STM32N6 chip and an MX25UM512G flash chip. The flash is connected identically to the Nucleo development board.When powering up the board in Dev Boot mode, it is not possible to read the flash chip u...

Nixxen by Associate II
  • 790 Views
  • 7 replies
  • 1 kudos

Resolved! STM32L4 USB Connectivity

Hello everyone. I am running into a USB Host <--> Device connectivity issue. I have 2 STM32L496 MCUs, one as Host and other as Device. I cannot get the CDC connectivity to work for some reason. The connections are as follows: D+ <> D+, D- <>D-, GND<>...

Resolved! STM32G05 ADC problems adding IN8, IN9 or IN10

Hi.I'm using an STM32G051 and would like to use 12 ADC channels which are not sequential. I have thus set up the ADC for 'sequencer set to not fully configurable' as show below:Ignore for the moment that IN9 is red, I think I was trying something wit...

stm32adc.png
GMeta.1 by Associate III
  • 282 Views
  • 2 replies
  • 0 kudos

STM32H5 VCORE drop detection

Hello, Is my understanding correct that it's impossible to internally detect short (<100ns) drops of VCORE internally? Reading RM0481 page 154 it seems impossible to directly monitor VCORE through the tamper mechanism which I assume forces the use of...

gquere by Associate
  • 315 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.