cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H5 VCORE drop detection

gquere
Associate

Hello,

Is my understanding correct that it's impossible to internally detect short (<100ns) drops of VCORE internally?

Reading RM0481 page 154 it seems impossible to directly monitor VCORE through the tamper mechanism which I assume forces the use of an ADC+WDG, which probably puts the detection range in the µs? Which means the target is sensitive to fault injections?

1 REPLY 1
KDJEM.1
ST Employee

Hello @gquere and welcome to the community;

 

As mentioned in the datasheet the minimum TS_VCore is 1 µs, with ADC sampling time when reading the VCORE voltage. Note that the VCORE monitoring characteristics value is specified by design and not tested in production.

KDJEM1_0-1775746371241.png

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.