2026-04-10 4:38 AM
Hi All,
I've this requirement, can someone suggest how do I proceed.
I'm using stm32u535 and over usart it's connected to Silicon labs chip. Silicon labs chip has Wi-Fi and I want to update firmware of STM32U535. This silicon labs chip is connected to cloud over Wi-Fi.
2026-04-10 5:20 AM
So you'll need to use a UART bootloader - either a custom one, or the System Bootloader (in ROM).
The STM32 neither knows nor cares what is on the other end of the link, so see:
How can I use an ESP32 to update the firmware of an STM32 from any family
Links to app notes in this reply
#FirmwareUpdate #IAP
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.