STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Data Buffer for serial and spi

hi hope have good dayi need to buffer data for save on every 1ms for serial and spi i use dma to receive datafor example hal_uart_receviveDMA on this function must set buffer size ...i test one example :50Hz send to mcu data each time 1000 and 1001 ...

MacLaren by Associate III
  • 4576 Views
  • 10 replies
  • 0 kudos

STM32H743 runs in debug mode only

Hi, I have several boards with same issue. After weeks of tests when flashing boards using STLink suddenly the micro is not running except in SWD debug mode. Flash is properly programmed but the micro is not running. A complete flash erase (all sec...

DGall by Associate II
  • 2746 Views
  • 3 replies
  • 0 kudos

Error working with stm32f030?

In a project I need to use an eeprom, I download st-s eeprom library for stm32f0xx ( AN4061 ). The provided example in keil mdk v4 had no errors however after I imported the eeprom.h and .c file in my own project in keil mdk v5 I started having probl...

AJava.5 by Associate
  • 907 Views
  • 0 replies
  • 0 kudos

STM32F030C8 I2C1 in BUS_BUSY after first start pulse.

First I thouht that problem in code generation from Cube, rewrote all in CMSIS, but nothing changed. I2C using only as a "slave", but after generation "start" and sending addres (0x70) + write no interrupt flags is set. Where my mistake?Initialisatio...

Wanderer by Associate
  • 896 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.