2020-02-03 9:02 PM
I am using stm32l432kc nucleo Board.
Is there any option for data retain when power is turned OFF ( Non-volatile memory Type).
If yes can you please share the details and sample codes
2020-02-04 3:23 AM
You can store data in the internal FLASH, just mind its erase granularity. Read the FLASH chapter in RM, and see examples in CubeL4.
JW
2020-02-04 5:32 AM
You may take a look at the X-CUBE-EEPROM EEPROM emulation library.
2020-02-04 5:53 AM
The internal flash has 2Kbytes erase blocks, so you can reserve some of them for storing data. Just decrease the flash size in the linker script e.g. by 8 Kbytes to give you 4 blocks at the end. See flash memory organization in the reference manual, and the user manual of your linker/toolchain.
There are a few drawbacks of using the internal flash though, it has a quite limited number of erase/write cycles, and writing/erasing the flash blocks program execution for a long time, nothing (not even interrupt code) runs while a flash sector is being erased.
There are 128 bytes of backup RAM available and preserved as long as there is battery power. Is there a battery holder on your board? This might be the simplest to configure and use, and you'd get a real time clock as a bonus.
And then it's possible to hook up an external $0.20 EEPROM IC.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.