STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

taking images from multiple cameras

I want to take videos from multiple cameras with stm and save these images to SD card. how is this possible?Is there a module you can recommend for this?

HTosu.1 by Associate
  • 753 Views
  • 0 replies
  • 0 kudos

STM32L072 (B-L072Z-LRWAN1) - SPI2 not working

Hi,I'm working with B-L072Z-LRWAN1 platform and struggle to see a signal on SPI2.My SPI2 is connected on an accelerometer. It is configured as follow:void HW_IMU_SPI_Init( void ) { /*##-1- Configure the SPI peripheral */ /* Set the SPI parameters...

NGugg.1 by Associate II
  • 1480 Views
  • 4 replies
  • 0 kudos

Not able to handle multiple external interrupts.

How to handle multiple External (more than 2 )interrupts on same port (eg Port A) of STM32. my code is below , I wants to know that how can I Differentiate External interrupt 0 And 1. I have configured pushbutton1 on PA0, Pushbutton2 on PA1, pushbutt...

STAR by Associate II
  • 3223 Views
  • 10 replies
  • 0 kudos

Best way to mate interrupts with c++ periephal drivers?

Hey!​Lets say I write general Can periephal driver in c++ for stm32f4 series(which I'm actually doing), then interrupt handlers for can1 and can2.​Now the proplem is how do I tell lets say can 1 rx interrupt, that >>this instance of object<< is the ...

JoniS by Senior
  • 5729 Views
  • 6 replies
  • 1 kudos

__set_BASEPRI -- implicit declaration

__set_PRIMASK(1); // No error __set_BASEPRI(3 << 4); // Implicit declarationThis is a snippet of my code from keil uvision5. But, the IDE results in a syntax error; implicit declaration of function ' __set_BASEPRI ' is inval...

0690X00000D8iehQAB.png
ASeyo by Associate II
  • 2886 Views
  • 3 replies
  • 0 kudos

Could you give me some reason, why after run receiving I2S via DMA, the handler at half and full of fill of a buffer runs only once?

Configuration: DIR9001 as reciever of optical sound and convertor to I2SSTM32F407VG DISCOVERYSTM32 CUBE IDEAfter setting I2S, I can normally at while loop recieve valid I2S singnal from convertor. After change code to DMA and starting the DMA via con...

DZimn.1 by Associate
  • 621 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.