STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Need help !!! I want to make 3 delay functions which works guaranteed delay in nanoSecond, microSecond and milliSeconds using Timer.

What i am currently using to achieve my goal.Few Details :1: STM32F103C8 Blue Pill2: CMISS core Library3:Datasheet, Reference Manual and Programming ManualI have attached two files. Which give you some idea that how I want to make These 3 functions. ...

Enabling a PWM kills ability to set state on some GPIOs

I am working with an STM32F777. I need to enable both GPIOs and PWMs (which ones is configured at run time by the application). Right now I'm seeing that some PWMs kill other GPIOs. For example if I turn on a PWM on TIM4 CH3 (PB8), it kills GPIOs on ...

CTack.1 by Associate
  • 1145 Views
  • 1 replies
  • 0 kudos

Resolved! Odd behavior in assembly busy wait cycle

I am preparing the labs for the undergraduate embedded systems course at the university where I work (the University of Milano-Bicocca in Italy). This year we will change the hardware and we will start using the STM32 Nucleo F767ZI boards. I am a tot...

PB1 by Associate III
  • 3200 Views
  • 13 replies
  • 0 kudos

Resolved! Variable Color Generation with PWM signals and RGB led.

Hello everybody.I tried to develop a simple application, using a RGB led to produce variable colors in a continous way along the time and I still not have succeeded completely. Let me explain what is happening:1) I used STM32CubeMX 5.3.0 to configure...

Can not open source input file: No such file or directory

Dear friends,I get a silly error " No such file or directory " in Keil IDE while I've already added the file path to include path directory of the compiler.This error happens only when I add lwIP source files to my project. And what's surprising is ...

0690X00000D8VEgQAN.png 0690X00000D8VEqQAN.png
Mujtaba by Senior
  • 4783 Views
  • 4 replies
  • 0 kudos

Resolved! STM32L433 LL SPI sending too much data (16 instead 8)

Hello. I need ability to send only 8 bit at the time. And I can't figure-out why I can send it, it keeps generating 16clocks no matter what LL_GPIO_ResetOutputPin(GPIOA,LL_GPIO_PIN_4); Delay(0x8); while((SPI1->SR&SPI_SR_TXE)!=SPI_SR_TXE); ...

Linas L by Senior II
  • 1771 Views
  • 4 replies
  • 0 kudos

STM32H7 SDMMC IDMA write multiple blocks error

Dear all,I am working with the sdmmc lib from STM and i am trying to get it working in DS (Default Speed @25Mhz) with a CARD_SDHC_SDXC, CARD_ULTRA_HIGH_SPEED sd card.When I write multiple blocks with the IDMA for the first time it’s no problem and ev...

STM32F411RE UART not working with IAR debugger

I am currently learning to work with stm32f411re. I use PA9/10 as TX and RX with baud rate 9600 and 1 start 8 bit word and 1 stop without parity. I connected PA9/PA10 with FTDI to my PC and i am trying to send from serial terminal. Trying to do this ...

AVuji.1 by Associate
  • 1711 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.