2019-08-17 12:18 AM
2019-08-17 8:13 AM
Are we sure that the Flash Loader Demonstrator is sufficiently recent to support G0.
Perhaps try the STM32 Cube Programmer in UART mode, as this is the tool that is being developed these days.
2019-08-17 8:13 AM
Are we sure that the Flash Loader Demonstrator is sufficiently recent to support G0.
Perhaps try the STM32 Cube Programmer in UART mode, as this is the tool that is being developed these days.
2019-08-17 12:57 PM
Use STM32 Cube Programmer
2020-02-10 12:03 AM
Hi Clive1: have Flash Demostator support STM32G0? please support me to make STmap file
2020-02-10 12:32 AM
Re-read the OP's question, and the given answers.
2020-02-10 12:43 AM
but It's 6 month ago, maybe now it's supported
2020-02-10 12:48 AM
You got that wrong.
The Flash Loader Demonstrator is abandoned by ST, in favour of the Cube Programmer.
There will be no updates.
2020-02-10 12:49 AM
thanks you for this update
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.