STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LPUART not work after SYS Clock Source change :(

Hello!. I Have two firmwares: bootloader and application. MCU is STM32L031K6U6First launched bootloader checking backdoor pin and launching appliction or starting firmware update process. If need just start firmware all work fine (bootloader don't ch...

Spider by Associate II
  • 1725 Views
  • 2 replies
  • 0 kudos

DMA interrupt on RX when get less the buffer size

Hello,I use DMA UART on Rx.but I get interrupts on half complete and full complete.is it possible to get interrupt earlier? when I get "\n" char?maybe the best way to mange is to use circular DMA, and when the half complete interrupt is fired, save t...

Lmali.1 by Associate III
  • 1594 Views
  • 5 replies
  • 0 kudos

How fast am I able to switch the alternate function on a given GPIO between a timer PWM output and GPIO during runtime?

I am using an STM32G4. I want to output PWM from a timer channel on one pin (call it pin A) and have a GPIO output on another (pin B). Then I want to be able to switch the functions on the two pins so that pin A is now a GPIO output and pin B is the...

Ricardo1 by Associate II
  • 1783 Views
  • 1 replies
  • 0 kudos

DMA2 HIFCR cannot be modified

This pertains to the Nucleo F446RE development board.I'm beginning to explore DMA and want to use it to drive a sine wave through DAC1. The code to "manually" feed the data works fine and I get the expected sine fine, I can see that on scope.So I'm n...

PWM channels of STM32G474. Is this the right MCU ?

Greetings,I need to provide PWM signals for 36 and 34 Outputs. Both the cases have been described under. Kindly note that all the outputs are independently operated. I need to know if STM32G474 can address to the job?CASE 1:These are the list of 6 PW...

JJ..1 by Associate II
  • 1677 Views
  • 1 replies
  • 0 kudos

WWDG_IRQHandler not waked up

hi, why WWDG_IRQHandler is not waking up, it configured even though not waking up.please guide me and show me asample program for WWDG.thanks

Cvadi.1 by Associate II
  • 2638 Views
  • 8 replies
  • 0 kudos

STM32f4 hterm problem

Hello, I am using hterm with stm32f4 to send and receive data. However, when receiving data streams, hterm hangs. I have tried everything but do not know what the problem is. Please help if you can.Thank you in advance

VYoun by Associate III
  • 1556 Views
  • 2 replies
  • 0 kudos

PWM generation with a phase shift on STM32F030R8T6?

Hi Guys, I am using TIM3 with 4 channels to generate a PWM signal for my motors. Right now there is no phase difference between the PWMs, but now there is a requirement where I need to generate a Phase difference like shown in the figure below I was ...

0690X00000D99QDQAZ.jpg

Resolved! Receiving wrong Data in UART in Nucleo Board.

Hi, I was testing UART communication using F446RE Nucleo Board. I was sending data to COM port by a python program running in PC and trying the receive to same data.ser.write(serial.to_bytes([1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15])) print...

SayanSeth by Associate II
  • 2919 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.