STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L552-EV, attempting to IAP program the flash through UART connection, however always fails to send the bin file through Y-modem protocol.

I've been using the example AN4657 and following it to a T. I'm using the example project library files form the STM32L476G IAP_Main and modified them where necessary to work with the 552.I can successfully connect to TeraTerm via usart3 connection a...

Rikerq by Associate II
  • 5040 Views
  • 5 replies
  • 0 kudos

ADC to DAC using DMA

If I set my sine wave generator to 1.5 Vpk-pk the DAC outputs a nice clean sine wave. If I increase the ADC input above that level, I start to see clipping of the sine wave. The negative part of the wave begins clipping before the positive part. Is t...

One Pulse Mode input can not be driven high enough.

Hello folks,Does any body know why the input pin can not be driven high enough when it is set as the trigger to TIM3 in OPM? I use CubeMX to generate the init code where TIM3 ch1 as input trigger and ch2 as the output. On the board, I use a comparato...

ming2 by Associate III
  • 3543 Views
  • 7 replies
  • 0 kudos

Resolved! How to reset TXE flag on SPI slave?

I'm simulating some issues on my STM32F412 DMA SPI SLAVE because I need to avoid any unrecoverable situation.If for any reason the TX is not empty (TXE is 0), I'm not able to reset it (set to 1) even reinitializing the peripheral.Probably, something ...

Guidoted by Associate III
  • 2258 Views
  • 4 replies
  • 0 kudos

stm32h7 spi interrupt latency

Hi all,I interfaced external(off board ADC) to stm32h743 microcontroller. i am receiveing data in spi interrupt mode. i enabled RXPIE interrupt.But the interrupt latency is increasing as Baud rate of SPI is increased.at lower speeds latency is small(...

kgang by Associate II
  • 3481 Views
  • 7 replies
  • 0 kudos

Running application from RAM

Hello,Is it that application can only run from ITCM ? When I try to run from other SRAM such as SRAM1, it get into MEM IRQ handler.Another issue is that on running from ITCM the HAL_Delay is much faster compared with running from internal flash (Xip...

ranran by Senior II
  • 3053 Views
  • 6 replies
  • 0 kudos

STM32F779NI internal ADC accuracy

I am using internal ADC of STM32F779NI connected to LMT86 Temperature sensor. Vref is 3.3v and ADC resolution used is 10-bit. The problem is there is always a difference with the expected ADC and the actual ADC for a given voltage. This difference is...

A3 by Associate III
  • 2873 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.