Ask questions, find answers, and share insights on STM32 products and their technical features.
I'm using stm32f103ze to send some data over the serial peripheral, but it didn't work. The settings are correctly set but when I try to write to the data register it always remains zero. Furthermore, none of the Serial peripherals seem to work. Wh...
I'm hoping this is a simple question. In the reference manual (RM0394 section 39.4.5), the tolerance of the LPUART receiver is specified in Table 204. For example, with BRR = 1024 and 9 bits/1 stop bit, the tolerance is given as 2.33%.I've been ass...
Hi,This is to request clarification on doubts regarding the storage of data in the non-volatile memory of the STM32G030C6T6 micro controller ... from what I see in the micro controller's technical sheet, it does not have EEPROM memory, since FLASH me...
Hi,I am trying to get some clarification on the accuracy of the STM32L4's HSI16. AN4736 mentions that the HSI16 will leave ST's factory calibrated to [-0.75%, 0.5%] at 30 C. DS11453 section 6.3.8 shows that the drift over 0 to 85 C will be -1% to 1...
I want to implement a timer which would elapse in 3s and gives me an interrupt then. But i want to build a kind of software watchdog which will be always reseted from an external clock 1s. So my idea is, when the external 1s clock is off then after 3...
sprintf(buffer,"Hello\r\n"); len=strlen(buffer); HAL_UART_Transmit(&huart1,(uint8_t *)buffer,strlen(buffer), 0xFFFF); HAL_Delay(100); // just in case required delay is given2. ch=83; HAL_UART_Transmit(&huart1, &ch...
I created a new project with the CubeMX for the STM32F205RC. I want to use the CAN-bus interface and use my old code (that uses the HAL library), but get a lot of errors. Seen the changelog and want to update my code, but the User manual for the HAL ...
Dear all, dear stm,we ported our project from stm32F427 to stm32F765 because we needed more RAM.After this we noticed that our code execution time has more than doubled.We check all twice, ART, Cache, Interrupt, PLL, etc.We tested also the Overdrive ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.