STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! EXTI PI2 not working on STM327508-DK

I have viewed every example on the internet, I think and seen many different commands and approaches. As long as the interrupt is disabled, the program works, but it crashes when enabled. Here are snippets related to EXTI. Maybe I have mixed code fro...

DRobe.4 by Senior
  • 1072 Views
  • 3 replies
  • 0 kudos

STM32F7 How to get 50MHz on GPIO

I can only get the GPIO pin to toggle at 8MHz but datasheet indicates 108MHz is possible.I tried changing OSPEEDRy[1:0] but this did not help, I only get the default 8MHz.

SRobs.1 by Associate II
  • 6473 Views
  • 20 replies
  • 0 kudos

Resolved! What does the data at the end of the inserted code mean when downloading the code?

Hello, everyone.I downloaded the code to STM32H753 and then used STM32 Community to look at the data on the flash memory and suddenly I got one question.I downloaded my code on flash memory bank 2 sector 0 (address 0x08100000) and found that the data...

0693W000000Tj0sQAC.png 0693W000000Tj0xQAC.png
Ekim.1 by Associate II
  • 1560 Views
  • 3 replies
  • 0 kudos

Resolved! STM32 ADC multiple channels HAL

Can some one tell me why this do not work?I start to freak out -.-..........I wish make 4 chanel adc with dma.Best Regards,Szymon

0690X00000DYubXQAT.jpg
STobo.1 by Associate II
  • 2071 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.