STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to transmit UART data on STM32 discovery board?

Hi forum, I'm developing on the stm32f3disovery board with STM32F3-Discovery_FW_V1.1.0 running in IAR Embedded Workbench. I've been able to get the basic demo compiled and running, but I can't seem to get UART data transmission to work. There are no ...

RLee.2 by Associate II
  • 3770 Views
  • 4 replies
  • 0 kudos

[SOLVED] --- Slidebar on STM32F746G-DISCO ----

Here my solution to create a slidebar on this evaluation board, it should run also in other STM32 modules.//###################################################################################### //# Slide bar //#######################################...

0693W000000UjCvQAK.jpg

Resolved! How to receive all data over UART interrupt?

I am using a STM32LO73RZ board. I have set up UART with interrupts and this works. I receive data that I send from an USB to TTL converter. When I sent a character one by one, this works fine. However, when I try to send a larger message, I keep miss...

Birdym by Associate II
  • 5313 Views
  • 7 replies
  • 0 kudos

Using Array to toggle outputs

Hi,I want to try use an array to set particulars outputs, base on values in that arraysI have initiated two dimensional array like in example below:uint8_t obrPr[4][4] = {  {0,0,1,1},  {1,1,0,0},  {0,1,1,0},  {1,0,0,1}   };This is sequences...

PZarc by Associate II
  • 1559 Views
  • 3 replies
  • 0 kudos

Resolved! RXFD_MODE and TXFD_MODE pins, what are they for?

STM32H745 DS indicates there are these signals:CANFD1_TXFD_MODECANFD1_RXFD_MODECANFD2_TXFD_MODECANFD2_RXFD_MODENo mention is made in the DS for their purpose, nor in AN5348 "FDCAN peripheral on STM32 devices". The signals are not mentioned at all in...

Hello, I need help in setting up a SPI3 communication with AT45DB161E flash memory using STM32H743II. My application gets stuck when trying to write/read data to the flash and I don't know why. Details and code can be found below. Thank you!

More details on the topic:I have a working application that runs with nuttx and is able to successfully configure SPI3 and read/write to the flash memoryI have compared the registers between my app(that doesn't work) and the application that runs wit...

BJurc.1 by Associate
  • 1102 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.