2020-03-14 12:36 PM
Section 24.3.8, page 752, third paragraph says:
"The inverting and non inverting inputs selection is performed using
the VPS_SEL and VMS_SEL bit fields in the OPAMP switch control register."
The "switch control register" should be "timer controlled mode register".
Sections 24.5.1 to 24.5.12 titles have "x" and (x = 1..6) in them that they shouldn't?
Examples:
24.5.1 OPAMP1 control/status register (OPAMPx_CSR) (x = 1...6)
should really be:
24.5.1 OPAMP1 control/status register (OPAMP1_CSR)
because there is a different one for OPAMP2:
24.5.2 OPAMP2 control/status register (OPAMPx_CSR) (x = 1...6)
this should be:
24.5.2 OPAMP2 control/status register (OPAMP2_CSR)
I haven't looked to see if the (x = 1..6) approach will work and all of them can be combined.
2020-03-16 12:38 AM
Hello,
Thank you for the remark
I will check
Regards
2020-03-25 5:04 AM
Hello
We will correct typos in the coming release of the RM.
Best Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.