Unrequested "upgrade"
Is it just me or did everyone else just suffer an unwanted unrequested "update" to their IDE?
Ask questions, find answers, and share insights on STM32 products and their technical features.
Is it just me or did everyone else just suffer an unwanted unrequested "update" to their IDE?
Hello. I was searching for information but I was unable to find clear answer. What is correct way to handle AT messages from gsm/bluetooth/gps modules ?I am making one product that will use at least two uart interfaces (SARA-R12) and NINA-W151 module...
Hi there,I am using the MCU STM32F103C8T6 and in my code I force an UsageFault condition but the UsageFault_Handler is not been called. I have enabled the USGFAULTENA bit in the SHCSR register, which enables the UsageFault. I envoked an UsageFault by...
Hi,I would like to use DMA request for USART1 RX and SPI1 RX. The AN4301 at section 4.3 states:Software sequence to enable DMAThe following software sequence applies when enabling DMA:Configure the suitable DMA stream.Enable the DMA stream used (set ...
But I can not return my message by CANLINE. When I do the same operations in STM32F103C8T6, I can get answers from the Canbus line.I chose the stm32f105RC family to use double canbus. I can't solve the problem. Do you have any ideas?. Thank you.
I am working on a STM32F746G-DISCO with I2C got on Arduino style board.I would like to reduce the I2C speed because sometime this lock my app with some external DAC chip.At this time I am using:CAMERA_IO_Init(); BSP_TS_Init(480, 272); and these...
I am developping a touch screen user interface to control an audio preampl and dac.I have no problems with I2C bus to set the registers of CT7302PL and ES9018K2M but if I try to read a single register the application hang.This is my I2C configuration...
currently i am using the stm32h743zi board.why pc8 and pc9 pins are not changed there transition state when they connected to 5v supply.
Hello,I am using stm32f4 discovery. I wrote 2 interrupts to blink LEDs in different speeds to write an example for NVIC. I have 1 question that I wonder about and 2 issues I couldn't solve. Here is the situation :All interrupts work well seperately. ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.