2020-03-27 10:27 AM
I am working on a STM32F746G-DISCO with I2C got on Arduino style board.
I would like to reduce the I2C speed because sometime this lock my app with some external DAC chip.
At this time I am using:
CAMERA_IO_Init();
BSP_TS_Init(480, 272);
and these function to read and write the reg on external DAC chip
CAMERA_IO_Write(0x90, 8, 0b10011001);
reg11 = CAMERA_IO_Read(0x90, 11);
2020-03-27 10:40 AM
The clock speed is set within the I2C initialization function. The relevant register is I2C->TIMINGR.
2020-03-27 11:03 PM
Probably I have found the point where to set it
Could you confirm this ?
static void I2Cx_Init(I2C_HandleTypeDef *i2c_handler)
{
if(HAL_I2C_GetState(i2c_handler) == HAL_I2C_STATE_RESET)
{
if (i2c_handler == (I2C_HandleTypeDef*)(&hI2cAudioHandler))
{
/* Audio and LCD I2C configuration */
i2c_handler->Instance = DISCOVERY_AUDIO_I2Cx;
//i2c_handler->Instance = DISCOVERY_EXT_I2Cx;
}
else
{
/* External, camera and Arduino connector I2C configuration */
i2c_handler->Instance = DISCOVERY_EXT_I2Cx;
}
#define DISCOVERY_I2Cx_TIMING_ORIG ((uint32_t)0x40912732)
#define DISCOVERY_I2Cx_TIMING_NEW ((uint32_t)0x10911823)
#define DISCOVERY_I2Cx_TIMING_NEW1 ((uint32_t)0x00611116)
i2c_handler->Init.Timing = DISCOVERY_I2Cx_TIMING_NEW1;
i2c_handler->Init.OwnAddress1 = 0;
i2c_handler->Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
i2c_handler->Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
i2c_handler->Init.OwnAddress2 = 0;
i2c_handler->Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
i2c_handler->Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
/* Init the I2C */
I2Cx_MspInit(i2c_handler);
HAL_I2C_Init(i2c_handler);
}
}
2020-03-27 11:31 PM
Why I have no I2C bus problems using the EXT/RF E2P connector (pin EXT_SDA/EXT_SCL) instead of CN7 connector (pin SDA/SCL) ?
Is this the point to modify the freq ?
//#define DISCOVERY_I2Cx_TIMING_ORIG ((uint32_t)0x40912732)
//#define DISCOVERY_I2Cx_TIMING_NEW ((uint32_t)0x10911823)
//#define DISCOVERY_I2Cx_TIMING_NEW1 ((uint32_t)0x00611116)
i2c_handler->Init.Timing = DISCOVERY_I2Cx_TIMING;
2020-03-28 10:26 AM
Here's what the code says about that parameter:
uint32_t Timing; /*!< Specifies the I2C_TIMINGR_register value.
This parameter calculated by referring to I2C initialization
section in Reference manual */
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.