STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4Px characteristics on the WWW page are false

On the page :https://www.st.com/content/st_com/en/products/microcontrollers-microprocessors/stm32-32-bit-arm-cortex-mcus/stm32-ultra-low-power-mcus/stm32l4-plus-series/stm32l4p5-q5.html?querycriteria=productId=LN2188$$1=STM32L4P5#then product selecto...

ADC self calibration, needed or not ?

Hello,I have a project where my ADC channels will be calibrated end of line using a calibration bench. I will directly calibrate the physical measurements (voltage and current). My question is: do I need to implement the ADC self-calibration sequence...

Stabilo by Associate III
  • 1551 Views
  • 2 replies
  • 0 kudos

Resolved! How to set ADC SOC at half of duty cycle Ton?

Hi,I'm designing a power supply using a stm32F334R8 Nucleo board. For the application is interesting to trigger the ADC SOC at half the Ton (In order to measure average current).I am using STM32CubeIde. I have read the reference manual and the HRTIM ...

0690X00000DXHrtQAH.png
mur by Associate III
  • 1264 Views
  • 1 replies
  • 0 kudos

Why FMC bus turnaround time is so long in mode D on STM32F303?

I'm using STM32F303ZE MCU's FMC(FSMC) to communicate with a special chip. FMC is cofigured in NOR/PSRAM mode, asynchronous, non multiplexed, timing mode D (see attached FMC configuration in CubeMX). FMC clock is equal to AHB MCU clock that is 70MHz. ...

0693W000000Uo8AQAS.jpg
RGris by Associate II
  • 3516 Views
  • 4 replies
  • 0 kudos

LPUART does not work

Helloi am using STM32 NECLEO-L010RB here i use low power uart (LPUART) so i try to send string on the terminal but i get garbage on the terminal so please provide me some example code.Thanks.

SMask.1 by Associate II
  • 3871 Views
  • 7 replies
  • 0 kudos

Resolved! PB5 remap pin on STM32F103C8

The pin PB5 used by SPI1 in REMAP mode conflicts with the SMBAl pin of i2c1, how to configure it as the MOSI function of SPI1 on STM32F103C8?PB5 seems to be used as SMBA by default when we use SPI1(remap mode) and i2c1 at the same time. Even if I con...

0693W000000UZykQAG.jpg
FHui.1 by Associate II
  • 6145 Views
  • 9 replies
  • 0 kudos

Write and read block on eMMC with DMA

I am using a STM32F411 and I want to write and read blocks on an 8 GB eMMC. There is no problem with the command part towards the eMMC but when I try to write a block of data it looks like the DMA never starts to move data to the fifo. Is there an e...

UHans.1 by Associate
  • 1230 Views
  • 0 replies
  • 0 kudos

Reading Acc. Values from lsm303dlhc (I2C)

I started a new project using CubeMX for my STM32F303-Discovery board and try to get the Acceleration values but without success!In my main.c, I do the following:i2cBuf[0]=0x20;//CTRL_REG1_A ODR = 1344HZ | Normal Mode | XZYeni2cBuf[1]=0x97;HAL_I2C_Ma...

Ala1980 by Associate II
  • 759 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.