STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Wrong voltage readings from ADC

Board: NUCLEO STM32F103RB - MB1136 C-01Hi all,I try read, trought ADC1_IN0 (pin PA0) , the temperauture value from LM35, but read wrong value.LM35: connected at 5V, GND and A0. ADC1_IN0: work at 8 MHz with voltage reference of 3.3V and 12 bit of reso...

Linux and custom code on dual core MCU

Hi EveryoneI'm wanting to have an STM32H747 run custom code on the M4 and Linux on the M7 with some basic interaction/messaging between the two.I've never attempted anything like this before and will be very grateful for any advice offered by the com...

JacquesV by Associate II
  • 3006 Views
  • 5 replies
  • 0 kudos

Import a projet to a different evaluation card

Hello,I am currently working on a project integrating the ST package (fp-aud-smartmic1) allowing to test acoustic improvement functions (echo cancellation, beamforming ...) however I wish to work on a different microcontroller than the one proposed i...

UTANG.1 by Associate II
  • 1301 Views
  • 3 replies
  • 0 kudos

Switch Block influencing stop2?

I'm seeing the following problem:In normal Mode, the current function to run, is from a swich/case block inside main();. This works perfectly fine in run mode. Some cases end up in STOP2, and change state (the switch/case) variable after the wakeup p...

STM32L010RB, STOPmode with RTC wakeup.

New to STM32 low power devices.I cannot get power consumption of the nucelo to below 120ua when measuring at IDD. I have configured the ISR and RTC as per NUCLEO-L031K6\Examples\PWR\PWR_STOP_RTCAny assistance would be highly appreciated. I can get th...

UART IT not working on STM32L0K8T6

Hey guys, i'm back.I'm trying to configure UART on STM32L0K8T6. The goal is just to send data to this MCU via TeraTerm and send data from MCU to PC.To do so, i used CUBEmx to easily configure UART but the fact is I can send data from MCU to PC but S...

0693W000000UqVaQAK.png
AJT by Associate III
  • 2045 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.