STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32f030cc clock exception

platform: stm32f030ccSDK: STM32F0xx_StdPeriph_Driver (V1.5.0)Startup file: startup_stm32f030xc.sClock configuration: Since the HSE external pins are made as ordinary GPIO ports, HSI is used as the system clock source. The configuration is as follows...

0693W000000W2lSQAS.bmp
Lyu.1 by Senior
  • 3395 Views
  • 10 replies
  • 0 kudos

Resolved! STM32H7,STM32H743 ADC with DMA

Posted on October 11, 2017 at 15:09In summer 2017, I started an project with the STM32F767 on the Nucleo board, because the H743 was still announced but not available. For some weeks I got the new Nucleo board of the STM32H743. After I transferred t...

Bug: RM0383 Reference manual

In RM0383 Reference manual on page 215 - Section: Continuous conversion mode.There is "SWSTRT bit" but shoul be "SWSTART bit".This is very important bit :-).

JSzem.1 by Associate II
  • 1853 Views
  • 3 replies
  • 1 kudos

ST, please unify the family graphics

On the individual families webpages, there's a clickable image-map, as a table of subfamilies together with their most prominent features.Recently, these underwent a facelift. Unfortunately, in some of them, the subfamilies are ordered top-to-bottom ...

0693W000000VZCsQAO.jpg 0693W000000VZEZQA4.jpg

Will my H743 chip handle 2 x 24 MHz, driven by 2 x SDI?

I have a Nucleo H743ZI2. I have been reading "Mastering STM32" by Carmine Noviello, and on page 188 (last paragraph) he says that the maximum IO toggle rate is 10 MHz on the STM32F446. He gives oscilloscope traces, but I can't see the frequency, beca...

MEwen.1 by Associate II
  • 5084 Views
  • 10 replies
  • 0 kudos

STM32F769 Disco DFSDM with DMA Maximum Transfer Length

Hello,Currently I am working on STM32F769 DISCO board with STM32CubeIDE, my aim is to transfer DFSDM conversion results to FMC RAM using DMA. I am able successfully transfer data and verify it. However, when my total conversion length goes above a li...

FP AI Sensing enable UART printf issue - sensortile

Halo,I am using sensortile and currently trying to be familiar with FP AI Sensing. There is an instruction to enable SENSING1_USE_PRINTF in SENSING1_config.h. I did enable it, however there is an error during compilation, and to solve I need to put S...

HKart by Associate II
  • 3761 Views
  • 6 replies
  • 1 kudos

Can I2C be assigned on CM4 and CM7 separately on STM32H747?

Hello, I am new to ST micro controller. We are now look for a suitable chip for our application. The STM32H747 has 4 ch I2C. Can I assign one I2C bus on CM4 core and another I2C bus on CM7 and these two I2C buses will talk to different system.Thanks,

AFung.1 by Associate II
  • 1743 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.