2020-04-15 4:54 PM
First sentence in the last paragraph says:
Up to 10 external event channels can be conditioned and are available simultaneously for
any of the 5 timers.
It should be 6 timers.
Actually, do a search for "5 timer" in Chapter 27 HRTIM and fix several locations that call out 5 timers instead of 6.
NOTE: use "5 timer" and not "5 timers" because there are places that are just timer.
Please also check the number of external event channels, etc. I didn't do that because I'm not very familiar with the implementation.
2020-04-16 12:35 AM
Hello,
Thank you, I will check
Best Regards
2020-04-22 4:11 AM
Hello,
Thank you for your contribution
I have raise your feedback internally for correction.
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.