STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G071/G081 stucked bit into unique ID?

I need to have a unique ID on 32bits. Unique ID of STM32G0x is on 96bits.It may have some stucked bit for '0', for example for XY wafer position, maybe others (lot #)?I've seen that " exact information about valid bits not fixed to 0 for given deciv...

THAUS.1 by Associate
  • 2704 Views
  • 5 replies
  • 0 kudos

UART with STM32F4xx Using USB to TTL Converter

I want to do UART by connecting USB to TTL converter(PN-USBTTL-FT, FTDI FT232RL) to Tx and Rx of the board pin without using the USB port of the debugger part of STM32F4xx.The main code is as follows:uint8_t a = 'a'; while (1) { HAL_UART_Transmit(&...

GKim.1 by Associate
  • 1990 Views
  • 1 replies
  • 0 kudos

CCM RAM use cases in STM32F4-series

Hi!It's a beginner question, but what is te purpose / use case the CCM RAM in STM32F4-series?I asking this due to CCM RAM in this MCUs connected to D-bus only. For this reason, this implementation don't have code execution capability nor DMA.I'm afra...

PTiha by Senior
  • 2936 Views
  • 3 replies
  • 0 kudos

Measure HSE using TIM17

We are using the STM32H753ZI and to test if the LSE and HSE have the correct frequency, we want to measure it's frequency using TIM16 and TIM17.We managed to measure the frequency of the LSE using the internal input capture of TIM16 but when we tried...

0693W000000VuMAQA0.png
rb1 by Associate II
  • 3945 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.