cancel
Showing results for 
Search instead for 
Did you mean: 

FP AI Sensing enable UART printf issue - sensortile

HKart
Associate II

Halo,

I am using sensortile and currently trying to be familiar with FP AI Sensing. There is an instruction to enable SENSING1_USE_PRINTF in SENSING1_config.h. I did enable it, however there is an error during compilation, and to solve I need to put SENSING1_USE_PWR_MGNT to 0.

The compilation has no error, however my teraterm COM port still doesnt receive any output from sensortile.

Anybody has tried this before?

Thank you

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
CPutt.1
Associate III

I am facing same issue...Did you make it work is it something to do with 10s delay?

HKart
Associate II

I didnt manage to make it work. I did confirm that it is not HW issue since I program other FW demo and the UART works.

So it must be the FW issue or I miss out something on the FW steps.

CPutt.1
Associate III

Did you try this initiallization. I will let you if I am able find it out.

CPutt.1
Associate III
 
CPutt.1
Associate III

I also tried it is not working for me as well

NOza.1
Associate II

Hello HKart,

Please find this link for the resolution of this issue.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.