STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Does STM32F730V8 support SDRAM or not?

It says specifically in datasheet that it does, but when I create new STM32CubeIDE project and select STM32F730V8, FMC only offers PSRAM/NOR Flash/LCD interface. I tried for testing purposes selecting some other MCU that also supposedly supports SDRA...

Slina by Associate III
  • 4711 Views
  • 13 replies
  • 0 kudos

Resolved! QUADSPI FLASH on STM32H747I-DISCO

I just would like to write/read to/from external flash on the development board and will really appreciate a hint how to make the easiest way. I have configured QUADSPI interface only for M7:QUADSPI Mode: Dual bank with qaurd linesChip Select for Du...

0693W000000WaIFQA0.png
ALevc.1 by Associate III
  • 2818 Views
  • 5 replies
  • 0 kudos

STM32F103RB Reliability

Hi all,I'm doing reliability analysis (according to Telcordia SR332 Issue 3 method) for a design and i need MTBF/FIT value for STM32F103RB.Best Regards

RVit by Associate
  • 978 Views
  • 1 replies
  • 0 kudos

Better way for mutlichannel ADC

Hello. I have stm32f407 MCU. I need read 6 ADC channels by timer (2 Khz) and store adc data to 6 circular buffers. What is better way do this?

TAndr.1 by Associate II
  • 2258 Views
  • 4 replies
  • 0 kudos

FLASH_CR address

Hi,I am developing a programmer over the SWD and need some advise. One of the tasks is to unlock the Flash with the unlock bit in the FLASH_CR register. I have found a reference manual and it says the offset is 0x10 but I can't find anywhere which st...

PMerc.1 by Associate II
  • 1712 Views
  • 4 replies
  • 0 kudos

STM32F7 CAN exit Sleep mode

I'm making my own low level CAN driver. I have a problem releasing the CANperipheral from sleep mode. So there are more requirements then I found so far. LL_AHB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_CAN1); LL_AHB3_GRP1_ForceReset(LL_APB1_GRP1_P...

Evan .1 by Associate II
  • 2016 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.