2020-04-24 8:11 AM
Hi,
I am developing a programmer over the SWD and need some advise. One of the tasks is to unlock the Flash with the unlock bit in the FLASH_CR register. I have found a reference manual and it says the offset is 0x10 but I can't find anywhere which states the base address.
Any assistance would be greatly recieved.
2020-04-24 8:14 AM
I should have said the specific device is a STM32F746
2020-04-27 3:05 AM
Thanks @PMerc.1
Indeed, I can then redirect the post to relevant topic to reach relevant community.
Hope someone can help you further there
Olivier
2020-04-28 12:21 AM
Hi Olivier,
Has this been redirected yet?
Paul
2020-04-28 1:21 AM
RM0385, section 2.2.2, Table 1, boundary address, "Flash interface register".
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.