STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to give delay when working gpio toggel?

Hello ,I am using Standard Peripheral Library with STM32F3VCT6 mcu. I want give delay without using timer of it means want give delay by using RCC clock. Is there any thing by which it can be happen.

LACTIC by Associate II
  • 2801 Views
  • 5 replies
  • 0 kudos

Resolved! Why HAL_UART_Transmit_DMA(&huart2, buffer, n) doesn't work properly inside Timer interrupt callback function?

Greeting Everyone,May I have some little help here? I'm currently using STM32F303K8. I had experimented with HAL_UART_Transmit_DMA function within "the main while loop" and the TIM6_DAC1_IRQHandler(void) which was called from TIM6 in Time Base modeMy...

0693W000000WXE0QAO.png
NNang.1 by Associate II
  • 2593 Views
  • 5 replies
  • 0 kudos

Resolved! STM32F103RCT6 simple blinking led problem.

Hi. First of all I want to thank you for giving time to this post. When i create bare metal program for blinking an LED don't work. The LED don't blink but when i enter DEBUG Mode with KEIL uVision the bit 0 in ODR resgister for GPIOC toggle every 1 ...

LDani.1 by Associate
  • 3418 Views
  • 3 replies
  • 0 kudos

X-NUCLEO-IDB05A1 fireware update field!

Hi, I is developing a BLE appilication using X-NUCLEO-IDB05A1 module. I use FlashUpdaterTool (Version 2.1.0) to connent my NUCLEO board of L476RG (VirtualCOMPort Application V0.0.1 ), which connect X-NUCLEO-IDB05A1 module. During updating the fire...

0693W000000WXfzQAG.png
xqiu.1 by Associate
  • 763 Views
  • 0 replies
  • 0 kudos

RTC second advanced and SSR greater than PREDIVS

Hi,​I​ am using stm32f779 RTC upto subseconds granularity that is using SSR register value for giving upto milliseconds level of time output .The scenario is such that there is external time source ( network clock) to which I synchronise RTC by updat...

A Maq by Senior
  • 1709 Views
  • 3 replies
  • 0 kudos

DMA Problem with USART

Hello,I have written these codes for transmitting an array to USART.1)The Message[21] Array fills up every 200us. It sets Flag=1 when data is ready.2) If the user makes the PB11 pin low it starts DMA section to transmit the data.(All data will transm...

parisa by Senior
  • 1283 Views
  • 1 replies
  • 0 kudos

Resolved! Starting timers in one pulse mode

Hello everyone,I read many of the posts on the forum and couldn't find an answer to this question: is there any way to start timers in one pulse mode other than through an external stimulus? that is, only through software? How could it be done?I am l...

LCatL by Associate II
  • 3587 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.