STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SDRAM configuration for 216MHz sysclk.

Hello, with a STM32F7508-DK board, all examples using SDRAM have the sysclk to 200MHz, therefore the FMC clock to 100MHz.I am trying to enable sysclk = 216MHz, and FMC = 108MHz, so I followed the SDRAM user manual, and configured the following settin...

VVasi.1 by Associate II
  • 2520 Views
  • 4 replies
  • 0 kudos

STM32L4 External SRAM problem

HiI am working with a STM32L496G_Discovery board and Cube IDEI am having problems with the external ram. I have called BSP_SRAM_Init();and defined an array in that ram spacefloat testInput[TEST_LENGTH_SAMPLES] __attribute__((section("._myvars")));In ...

Division by zero exception flag not set in STM32H7 FPU

I'm digging into the FPU of a STM32H743 (Nucleo board, Keil IDE).I've checked that the FPU is enabled in register CPACR.I've compiled the following dumb code:volatile double test = 0;   test = 1.0 / test;If I look at the assembly I've got:VDIV.F64 d0...

Gpeti by Senior II
  • 5597 Views
  • 9 replies
  • 0 kudos

STM32F103 HAL UART Receive Interrupt not working

Hi,I am using STM32F103 controller UART peripheral for serial communication.Using interrupt for receiving data. I am able to send data but not receiving any data using UART interrupt handler. Once the function entered inside the interrupt handler ge...

AOuse.1 by Associate
  • 2872 Views
  • 3 replies
  • 0 kudos

STM32H753XIH6: clarification on pins F1, F2, G2

For the TFBGA240+25 package:Page 62 says F2 is NCPage 64 says F2 is VSSWhich is correct?F1 and G2 are always referred as NC pins, but deep in a footnote (referenced on page 64, footnote appears on page 87) it says to connect these pins to VSS.I would...

inojosh by Associate III
  • 1460 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.