2020-06-02 8:40 AM
Hi
I am working with a STM32L496G_Discovery board and Cube IDE
I am having problems with the external ram. I have called BSP_SRAM_Init();
and defined an array in that ram space
float testInput[TEST_LENGTH_SAMPLES] __attribute__((section("._myvars")));
In my linker file I have
MEM_BASE (xrw) : ORIGIN = 0x60000000, LENGTH = 1024K
and
._myvars(NOLOAD) : {*(._myvars)} >MEM_BASE
But I can only get NaNs in that ram space.
I did something similar with a ST32L476 EVAL board and that worked successfully
Thank you
developerR
2020-06-02 8:52 AM
NOLOAD is the NOINIT / No Initialize directive, nothing is going to get into ELF file describing the actual content.
Content would need to be directed into FLASH, you'd need to bounds the static data with symbols in the linker script, and add code in startup.s to unpack it into the the External SRAM after you've brought up the pins/interface.
Keil would do more of this automatically, but you're using GNU tools and these are a lot rougher around the edges.
2020-06-02 11:15 AM
To me, this sounds more like the FMC is not initialized properly.
Can you "see" the memory in debugger? Are FMC regsiters set appropriately?
The 'L496 Disco has a rather involved power supply scheme. Is VDD jumpered to 3.3V? Is PH0=LCD_PWR_ON set?
JW
2020-06-03 3:26 AM
thanks folks for your input
this was my issue
#define SRAM_DEVICE_ADDR ((uint32_t)0x60000000) eval
#define SRAM_DEVICE_ADDR ((uint32_t)0x64000000) disco
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.