STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

When setting up pins to communicate using SPI on a sensortile I changed the Pins so one is the C and one the B GPIO, how would I set this up, I haeve only seen one somewhat related thread that wasn't comparable, thanks!

GPIO_InitTypeDef GPIO_InitStruct; /* USER CODE BEGIN SPI2_MspInit 0 */ /* USER CODE END SPI2_MspInit 0 */  /* Enable Peripheral clock */  __HAL_RCC_SPI2_CLK_ENABLE();  __HAL_RCC_GPIOB_CLK_ENABLE();    /**SPI2 GPIO Configuration     PB15   ------> SPI...

AMell.1 by Associate III
  • 1249 Views
  • 1 replies
  • 0 kudos

Why my timer encoder mode oscillates in the same values?

Hi, i'm using my STM32F7 nucleo 144 and i'm learning about timer encoder mode and i follow the example in the datasheet but when i check the CNT register it oscillates in the same values and if i use the A0-A1 pins the encoder works bad, can somebody...

ARami.8 by Associate II
  • 2977 Views
  • 4 replies
  • 0 kudos

STM32L452RE ADC Bad value on just one of the 9 channels

I have STM32L452RET6P running at 1.8V, 24MHz. I am using nine ADC1 channels and am getting a very low value (about half) on ADC1-1 (PC0).All inputs are set up the same way, with an RC filter (33kOhm/0.1uF). The sampling rate cycle is 12.5 at 10bits, ...

JHong.1 by Associate
  • 1213 Views
  • 3 replies
  • 0 kudos

Resolved! SPI interrupt too slow for SPI frequency

I need to confirm my understanding. Say that my STM32H7 SPI is setup as Slave and that it processes the incoming SPI data byte per byte in interruption. It is very likely to happen that the SPI throughput is faster than the SPI interrupt handler dura...

Gpeti by Senior II
  • 1186 Views
  • 1 replies
  • 0 kudos

how CAN memory works?

Hello everyone i am using CAN bus to connect two stm32 boards, i would like to know does anyone of you know how does the CAN memory works? is it DMA or what exactly? i couldn't manage to find anyuthing on the internet and i really hope one of you can...

SGUIG.1 by Associate II
  • 2478 Views
  • 4 replies
  • 0 kudos

Data transfer between CAN bus and DMA on Hal stm32F4

hello everyone, i would like to know how can i transfer data from CAN Bus to DMA memory on stm32f4 board on HAL Library?  also i want to make sure that the CAN access memory is it DMA or somethign else?can you please explain to me how? or if you hav...

SGUIG.1 by Associate II
  • 4558 Views
  • 4 replies
  • 0 kudos

Resolved! Rx lane not receiving

Hello, I try to make an UART communication between Nucleo STM32F030RE and a STM32F030K6 mounted on a custom pcb.sends from NUCLEO to STM32F030K6 is OKReceive from STM32F030K6 is ok sends from STM32F030K6 to NUCLEO is OK (i can check it and decode tha...

JGreg.2 by Associate III
  • 2206 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.